FOR IMMEDIATE RELEASE No. 3209
Enables high-speed data transmission and reduced power consumption within mobile networks
TOKYO, September 4, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of a 25Gbps EML CAN module supporting high-speed optical data transmission in radio access networks within fifth-generation (5G) mobile base stations. The new module will be on display at the China International Optoelectronic Exposition (CIOE) 2018 in Shenzhen, China, from September 5 to 8, and will be commercially available from November 1.
Product | Model | Wavelength | Operating case temperture range |
Shipment date |
---|---|---|---|---|
25Gbps EML CAN |
ML760B54 | 1270nm, 1310nm |
- 40℃ to + 95℃ | November 1, 2018 |
The introduction of 5G mobile networks will herald the transmission of huge volumes of data and the need for high-speed optical communication networks; this will in turn drive customer demand for high-speed optical devices with low power consumption. The new 25Gbps EML CAN unit addresses these requirements, and will help to improve the productivity and efficiency of customer installations.
Note that the releases are accurate at the time of publication but may be subject to change without notice.