News Releases

Mitsubishi Electric to Ship Samples of 80x60-pixel Thermal-diode Infrared Sensor Capable of Measuring Temperatures up to 200 degrees CelsiusAccurately measures high temperatures in kitchens and factories for enhanced convenience and safety

FOR IMMEDIATE RELEASE No. 3561

Thermal-diode infrared sensor (MelDIR) capable of measurements up to 200°C


TOKYO, December 6, 2022 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will begin shipping samples of a new thermal sensor capable of measurements up to 200°C on February 1, 2023.
The company's existing MelDIR, launched in 2019, measures temperatures from -5°C to 60°C for applications including heating, ventilation and air conditioning (HVAC), security, people counting, and smart buildings. In response to demands for measuring higher temperatures in kitchens and factories, however, the new MelDIR "MIR8060B3" uses advanced signal processing and an optimized lens to measure temperatures up to 200°C. It also is expected to help shorten the lead time between product planning and production by user support tools such as thermal- imaging examples, demonstration kits and reference designs.1



  1. *Information for software and hardware design

Note

Note that the press releases are accurate at the time of publication but may be subject to change without notice.


Inquiry

Media contact

Customer Inquiries